This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSEVM6657: Using EVM with TMDXEVMPCI

Part Number: TMDSEVM6657
Other Parts Discussed in Thread: TMDXEVMPCI,

We are using the TMDSEVM6657 in our development. I would like to use it to exercise the PCIe but I’m told that the connections for PCIe on that board are to the AMC (card edge) connector. I did also come across the TMDXEVMPCI AMC to PCIe Adapter card. That looked hopeful but on that one the supported products list does not include the 6657. Is there a version that works with the 6657, or a workaround? Is it possible to use this adapter card with that Evaluation board?