Part Number: ADS122C04
Other Parts Discussed in Thread: LSF0204,
When using the ADS122C04 I2C Interface with the LSF0204, what is the current sink capability at SCL/SDA pins?
Background of this question: We want to use the device with a “switch-based” level-shifter (LSF0204) which requires the i2c slaves to be able to sink current (up to ~3mA).
I guess as these are CMOS input's the 3mA sound high. If LSF0204 is not working is there any suggestion on a pin compatible device?