Part Number: ADS127L01
Other Parts Discussed in Thread: ADS124S08, ADS1261, , ADS127L11, , THS4551
We are designing a strain gauge based sensing circuit and need to make both static (signal unchanged or slowly changing around 30-60 seconds) and dynamic (signal vibrates around ~1kHz) measurement as accurate as possible. The entire circuit is currently designed to be powered by a 3.3V battery so that limits my options for the ADC. I am aware of the more integrated solution such as ADS124S08 (only 4-kSPS) and ADS1261 (only 40-kSPS) but their sampling rate won't resolve my 1kHz signal changes. I'm drawn into the 512kSPS of ADS127L01 and even at low-power mode it offers up to 128kSPS - so that should take care of my needed sampling rate. It also operates under 3V so that'll work well with my 3.3V and my LDO. I'm not sure what could be my trade off for using a high-speed ADC for this application - e.g. does it take away some stability while making static measurement (bad drift over short time)? Is it a good choice for static and dynamic strain gauge or are there better alternatives for low-voltage/battery power supply?