This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS7128: Does this device incorporate an buffer for the 4 analog inputs?

Part Number: ADS7128


Is there an input buffer on these two devices, TLA2528I  and  ADS7128, to isolate the A/D convertors from the outside world?  I am unable to find any reference in the data sheet.  I am scaling the input to the devices with a resistive divider and want to make certain that I will not be introducing an error with a 4.7k source impedance.

  • Hello,

    The block diagram in the datasheet is an accurate representation of the device architecture. There is no integrated input in these devices. 

    Using resistor dividers to step down a high input voltage is a common use for this device. The measurement will be as good as the input signal, but any known error or deviation can be taken into account within the host device. 

    I suggest looking at the following short document: Driving a SAR directly without a buffer ~click here~, this will provide good generation information, though not specific to a resistor divider

      

    Regards

    Cynthia