This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Source for MMB0, ADS1289 and ADS1178

Other Parts Discussed in Thread: ADS1298, ADS1178, ADS1298ECGFE-PDK

Hi,

I've just received the ADS1298 kit and I would also very much appreciate the source code for the MMB0 board.

I'm also working with the ADS1178 on the MMB0 board, would it be possible to get the source code for controlling this board as well ?

My email is s053029 at student.dtu.dk

Thanks in advance

Kind Regards

Lasse Hansen

  • Hi Lasse,

    Welcome to the E2E forums! Glad to see you've taken interest in some of our components. This code was written in CCSv3.3, conversion to CCSv4 is a non-trivial matter. Many of the built in libraries and features of CCSv3.3 are no longer included by default for CCSv4. You're going to have to change a lot of include paths, add the CSL, and add the supporting libraries for DSP BIOS if you wish to use CCSv4.

     

    8764.Source Code.zip

  • I am also testing the ADS1298 with the ADS1298ECGFE-PDK and would like to see how the communication with the ADS1298 is actually implemented in the code for the mmb0, and to try to modify a few things to see how can I adapt it to the system I am designing. For that i also need the source code and an environment that makes it easy to make changes and see their effect. Is your answer from May 2011 still valid in November 2013? If it is, could you guide me to where exactly I can download the CCSv3.3 that the current code was last compiled with? Thanks!

  • Julio -

    Yes, the previous post still is correct.  Unfortunately, I don't think CCS3.3 is available for outside us, but we will check to see if there is something we can do.

    In the meantime, may we contact you offline to attempt to resolve your questions?  We typically use the email address in your profile.

  • Absolutely! You can contact me to my email on file. I really want to see how changing some details of the way you guys communicate with the ADS1298 affect its performance and data integrity and for that I'll need to make simple changes to the code. Without the correct IDE, it'd take me too long and won't be able to fit the evaluation in the schedule I'm committed on delivering. The product I'm working on will be a mass distribution product. Basically it is a patented new technology to assess patients with suspected heart disease and its based on continuous monitoring of those patients. In practice everybody and their mother :) will want to use this assessment.

  • You should receive an email with further information shortly.