Part Number: ADS114S06B
Hi,
I have selected ADS114S06B 16 bit ADC for my application. My requirement is to read temperature from 0 deg centigrade to 60 deg centigrade with a accuracy 0.005 degrees and 1% tolerance . As it is 16 bit ADC, and I want to select 5V as reference voltage.
1LSB that I can read for 16 bit and 5V reference is equal to 5/POW (2,16) -1 which corresponds to 76.29 micro volts. My question is am I able to acheive 0.005 degree accuracy with this output or not. Please suggest.
Regards,
Mark Steve