Other Parts Discussed in Thread: TX7332,
Is there some code I can look at or tutorial I can follow to set the AFE profiles? I am very new to this and I am a student. I have the AFE5832LP and TX7332. I understand that I need to set the profiles for these devices using an FPGA through the SPI interface. How do I set the register values using the FPGA and send that to the AFE/Pulser? Thank you so much for the help.