This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1602: Datasheet question asking

Part Number: ADS1602

Hi team,

My customer has some question would like to ask, please see below questions.

1.) It is recommended to use OSC for CLK input, and if there are multiple ADS1602s, the CLK should be connected to each IC in parallel. Does this CLK need to be connected to the control IC after the ADC? (such as MCU, FPGA, CPU...etc)

2.) Based on the above question, if CLK is not connected to the control IC after the ADC, how can the control IC send the SYNC signal at the CLK falling edge?

3.) When the system is powered on, the control IC only needs to send SYNC, and then ADS1602 will send FSO/SCLK/DOUT by itself? What is the sequence between CLK, SCLK and SYNC?

4.) According to the spec, can the input of AINP&AINN only be +2.95~-0.05V?