Part Number: ADS1299-4
Hi team,
I want to configure ADS1299-4 in Fully Differential mode with common mode voltage at 0V [(AVDD + AVSS) / 2]. AVDD = 2.5V and AVSS = -2.5V.
I'm using internal Vref = 4.5V with VREFN = AVSS = -2.5V.
With this VREFP = AVSS + 4.5 = 2V
VREFN = AVSS = -2.5V
So , as per datasheet section 9.3.1.2 Analog Input , differential input range can span from –VREF / gain to VREF / gain . If I consider PGA Gain = 1 , does that mean my input range will be from -4.5V to +4.5V [9V swing].
Ans similarly if PGA Gain = 2 , does that mean my input range will be from -2.25V to +2.25V.
Or is it a typo error and should be like –VREFN / gain to VREFP / gain ? so that for PGA Gain =1 , it will be like , -2.5V to +2V ?
Please suggest
Thank You