Part Number: AFE4410
Other Parts Discussed in Thread: AFE4500
Team,
Customer report there is a wearable project which can monitor the water loss in human body used AD5940, but meet some issue.
I would like to promote our AFE4410 to replace the competitor AD5940, can you help with a comparison of the main parameters between AD5940 and AFE4410? Or do you have another advice alternative part?
The application spec are as follows:
1. Measure the resistance of the two resistors (resistance 1, resistance 2) respectively, the resistance measurement requires a range of 10~150K, and the actual range can be larger
2. The fastest sampling time is 500 milliseconds to measure the resistance value (resistance 1, 2)
3. The reference application of AD5940 is 2-wire bioimpedance: www.analog.com/.../an-1557.html
Do we have such a similar application? Is there a reference circuit for AFE4410, preferably PIN: VXO as a multi-channel analog output?
Thanks for your support.
Best regards,
William