I am using the ADS124S08 in a differential channel configuration. If I set the reference, gain sample rate and filter type the same for the channels I am using and only switching the input multiplexer between channels to read the channels I need, will the converter run faster if I do not change anything except the input multiplexer or does changing the input multiplexer change the settling time of the converter and make it the longer first conversion value?