Part Number: ADS54J66EVM
Other Parts Discussed in Thread: DAC38RF82
Hi team,
I got a question from customer.
"
Does the deterministic delay in JESD204B Subclass 1 means that, the 1st sample points that the logical device received are about same after different times power-up?
Like, the input analog signals are free-run, the radian of sampled siganls is 0.5 at assumption, and the sample time is 5s delay after power up and configuring. Unpluged and re-power up, is that the radian equal to 0.5, when signals are sampled at 5s or 10s delay after power up and configuring?
"
Thank you very much for your help.
Best regards,