Hello, TI staff,
I designed 24 channels DAC board on which 24 DAC8811ICDGKTs were used.
TPn(n=1-to-24) are the outputs of OPamps which are connected to the outputs of DAC8811s as I/V converter.
I measured TPn after power-up. The results were that TPn of 21 channels were 0V but those of 3 channels were not 0V.
And their values of 3 channels changed every measurement.
The measurements were done under the conditions that SPI interface (CLK/CSb/SDI) was all floating.
These pins have no pull-up resistors and were not connected to controller (FPGA).
Please teach me the method to get TPn=0V on power-up certainly.
(1) Even though SPI interface is not connected to controller, pulling up CLK, CSb, and SDI to VDD with resistors (4.7kohm-10kohm) leads to TPn=0V?
(2) Do the following parameters affect power-on reset?
(a) the ramp rate of VDD
(b) the power supply sequence between VDD (DAC8811) and OPamp
Rigards,