Part Number: DAC8775
Hi team,
I would like to understand more on ALARM and Status Register Pin functionality in detecting open circuit condition in current mode o/p. Once the Fault is detected through ALARM pin and Open wire condition is determined by using Status Register 0x0B (bit3:0).
- Can we use this method to determine the open wire condition?
- Here Fault Channel x (X=A,B,C,D) indicated fault on respective channel. In this context, Does channel Fault meaning either short circuit for voltage mode or open circuit for current mode?
- Are there any other faults other than open circuit/ short circuit channel faults?
- I am using EVM to determine the open wire condition. I configured one of the channel in current mode. (Data loaded F). I removed the jumper on the o/p to simulate open wire condition. I have not observed any alarm when removed the jumper on the channel and Status register did not show any fault. What is the minimum current is required to determine the open wire condition in this case?