This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE7222: Test patterns synchronization, DDR sample output sequence

Part Number: AFE7222

I'm using the AFE7222 in CMOS mode. 

Are the test patterns on the two channels synchronized in any way (or is there a way to get them synchronized)? If I put both into TOGGLE mode, I'd like both channels to read 555 or AAA at the same time. If I put them into RAMP mode, I'd like them to roll over at the same time to the next value.

Also, to clarify, in CMOS DDR mode, let's say sample 0 is taken by ADC A and B on a single clock edge, giving two samples A0 and B0 (followed by A1/B1, A2/B2, etc). Will A0 be driven on the rising edge BEFORE B0 on the next falling edge? Or will B0 be on the falling edge immediately preceding A0? 

In other words, will the sequence look like:

B0 A0 B1 A1 B2 A2

or

xx A0 B0 A1 B1 A2 B2

Thanks!