Part Number: DAC53508
Other Parts Discussed in Thread: DAC53204, DAC53608
- DAC53508 for Adjust the TPS62816QWRWYRQ1 DC-DC Output Voltage
- * for Channels that are not in use - can I leave them float (not connected) or should I connect them to GND
2. for Adjustment of dual DCDC LM5143QRWGRQ1 Output Voltage:
- Since I didn't see any application note for Adjust Vout under this component, do you recommend using the same technique with DAC?·
- If yes, DAC53508 should be OK?·
- If not, can I use a digital potentiometer in series to the feedback resistor R2?