Other Parts Discussed in Thread: ADS1258, OPA350, OPA2365
Hello,
this week I was facing the problem that I read a rather noisy sensor signal with my ADS1258. I wanted to verify that my reference voltage is not the problem, so i logged the Vref reading. On the Vref reading I also had a rather big noise (1mV on the 5V reference). Still, I could not find a reason why there should be so much noise in the system, so I started to doubt the Vref reading and connected Vref with a short wire to an analog input of the ADC where I then measured much less noise on Vref (something like 50µV, which is quite reasonable with my settling time and data rate settings).
My question is: is it true that the Vref reading is not actually measured with the same resolution as the analog inputs, or do I possibly have some other issue in the system?
Regards.
Norman