This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1299-4: ADs1299-4

Part Number: ADS1299-4
Other Parts Discussed in Thread: ADS1299

Hi team

I am working of the EEG(AFE) ADS1299

 I am using  the signal conditioning circuit preamplification stage before the ADS1299.

As i am using the single channel (IN1P) as data, SRB, BIAS electrodes from the open BCI captured the Data 

But i have a question  when i use the Instrumentation amplifier for the +Ve (IN+) I will connect the electrode for the Negative of the Instrumentation amplifier I will use  the SRB is it correct 

If yes what is the reference voltage on the SRB pin.