This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8330: Best way to power +VA?

Part Number: ADS8330


I'm curious what the exact purpose of +VA is, like, what is it powering? 

Does it need to be a low ripple source? 
If yes, can I just power it from my voltage reference or is that a stupid thing to do? 

The voltage reference I'm using is the REF5040AIDR which is rated for 10mA output. This ADC is the only thing using that ref.