Part Number: ADS1115EVM-PDK
Hello,
I recently purchased the ADS1115V2EVM-PDK. When I went to install the GUI, I noticed that it runs "in the cloud" <gulp>. I went ahead and installed the browser extension and ithen nstalled the *.exe package. I then plugged in the board and went to the ADS1115V2EVM-PDK page where you press the "Evaluate In The Cloud" button to start the GUI (again, <gulp>). However, I receive the error below:
"! ERROR: Connection to BULK device timed out...."
(I tried to insert a screenshot, but the E2E site wouldn't allow me to Insert->Image)
I then tried to connect manually by doing Options->Serial Port. I see the COM port knows the PAMB is connected, so I go ahead and click "OK". The little in the upper left goes green for about 2-3 seconds, but then I get the same error as above.
Any idea what could be causing this?
Regards,
Mark