This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC80508: Overshoot or Peaking observed in Waveform outputs of DAC

Part Number: DAC80508

Hi We are using DAC80508 in our design. We are seeing an over shoot or peaking at leading edge while generating waveforms. This is irrespective of loads (we isolated loads and checked, we see peaking at that condition too).
We see the peaking consistantly from 0V to 4V. Beyond 4V, this peaking disappears. Also the peaking is seen only in the first pulse of waveform sequence.


If we introduce offset to the waveforms then the peaking disapperas.

This observation is seen in all channels of the DAC. This is not accepted for our requirement. So we would like to know reason for this behaviour of DAC. Is this expected from DAC or do you think there is some other reasons for this observation.
Also suggest any changes needed in the circuit.


The schematics of DAC is attached here. The waveform of peaking observed is also shown here.