Part Number: AMC60304
Dears
I have a project for Optical module 400G QSFP-DD DR4
need One laser support 4-way output so i need Idac>400mA.
Can AMC60304 IDAC two channels are combined into one channel, and the output reaches 400mA??
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AMC60304
Dears
I have a project for Optical module 400G QSFP-DD DR4
need One laser support 4-way output so i need Idac>400mA.
Can AMC60304 IDAC two channels are combined into one channel, and the output reaches 400mA??
Hi,
For applications that require additional current greater than the current provided by a single channel, multiple
IDACs can be used in parallel. Multiple IDAC channels can be shorted together to produce a current that is
equal to the sum of the individual channels. Make sure that the connected channels are enabled and disabled
simultaneously. Avoid scenarios where a single change channel is enabled or disabled. Also make sure that
the current being sourced by both channels is approximately the same to allow for evenly distributed heat
dissipation.
Regards,
AK