This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

VSP5610: Unused pins

Part Number: VSP5610

Hi Team,

Could you tell me how we should deal with following pins if unused?

PIN NUMBER TERMINAL NAME  TYPE(1) DESCRIPTIONS Unused?
13 REF_AIN AI3.3 /AO3.3 REF_DAC_IN = "0": Analog signal reference output (default)
REF_DAC_IN = "1": Analog signal reference input
Left floating?
20 XSH1 DO3.3 Sensor shift gate output 1 Left floating?
21 XSH2 DO3.3 Sensor shift gate output 2 Left floating?
22 XSH3 DO3.3 Sensor shift gate output 3 Left floating?
23 XSH4 DO3.3 Sensor shift gate output 4 Left floating?
48 XCLR DO3.3 Sensor clear gate output Left floating?
49 XP1 DO3.3 Fast transfer clock output φ1 Left floating?
50 XP2 DO3.3 Fast transfer clock output φ2 Left floating?
51 XP3 DO3.3 Fast transfer clock output φ3 Left floating?
52 XP4 DO3.3 Fast transfer clock output φ4 Left floating?
53 X1L DO3.3 Fast transfer clock output 1L Left floating?
54 X2L DO3.3 Fast transfer clock output 2L Left floating?
55 XCP DO3.3 Clamp gate clock output Left floating?
56 XRS DO3.3 Reset gate clock output Left floating?

Regards,

Takashi Onawa