Hello,
My project is having problems to read the Ads8665 spi credibility, and to know if the
ads8665 has in fact even booted.
The data sheet states that RVS should go high 20 ms after RST/ goes High.
If also, I raise the cs/ to High, Rvs also goes High, but there is no evidence
of a successful default setup Adc read. Also, there is no evidence of a successful
register read.
May I conclude that RVS must go High with CS/ Low in order to know that this
Ic has booted?
If the boot has failed, as above, what are the possible reasons that the ads8665 might fail to boot??
Thank you for your time and consideration.
Regards,