Other Parts Discussed in Thread: DAC3282EVM, DAC3282
The goal is to load my own external pattern file (a sinus with square waves) in the TSW1400EVM to generate the signal in the DAC3282EVM, but first i try just generating my own sinus.
I am using the ouput J1 and J3 of the DAC3282EVM and to do so I moved the jumpers as explained in section 4.1 in DAC user's guide.
Loading an external pattern file generated with the MultiTone generator works and i can see the output on a spectrum analyzer. But when i try to load my own pattern file, nothing comes out from J1 or J3 outputs of DAC3282EVM even though the file is well generated in the HSDC Pro.
This is my pattern file :
And this is what I get on the HSDC Pro, my file loads well :
Can u helps please ?
Thanks