This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC7750: A new device for daisy chain.

Guru 10720 points
Part Number: DAC7750
Other Parts Discussed in Thread: DAC8775, DAC8771

Hi team,

DAC7750 can't daisy chain in the datasheet, so I'm looking for a new device that can daisy chain.
Do you have any recommended devices for 4 - 20mA?

Sincerely.
Kengo.

  • Kengo,

    Instead of using a daisy chain, I would consider using a device with multiple channels, and a single SPI interface. One possible device to use the DAC8775. This device has four channels that can be used as either voltage output or current output. 

    If that's too many channels, I believe that the single channel DAC8771 can be used in a daisy chain configuration.

    Joseph Wu