Part Number: DAC7718
Hi all, I have two questions regarding the GPIO Pins.
- I'm trying to desing the startup sequence and was wondering if the GPIO Pins and SPI registers are already available without the analog power supply (AVDD), so that I can use one GPIO from the DAC7718 to Power Up his own analog power supply (AVDD) via the Microcontroller and the SPI register of the DAC7718.
- I want to clearify if I understand that correctly: If the devices power up(or is off) the GPIO pins are tied to high-impedance. So when I'm using pull-up resistor there is the power supply voltage (IOVDD) on the GPIO Pin if the device is turned off? And I can only set them active to low --> 0V
Best Wishes
Jonas