Other Parts Discussed in Thread: ADS62P49
Hello,
I'm just designing an ADC board based on the ADS62P49. It's going to work with 250MSPS with the two channel. The previous stage is a DGA that cames from a 2.4 GHz Front-End. The DGA has a differential output and fix the common mode voltage in a range from 1.6 to 2V.
For that reason I think that, in the ADC, I would need to fix the CM externaly taking the voltage from the previous stage. The problem is that if I want to configurate the ADC in serial mode way, at the beginning, before write the external mode value in the corresponding register, it may be configured with an internal reference and in the CM will be two references at the same time trying to fix it's value.
¿Is it really how I think or I can fix an external reference and configurate it in serial mode without any problem?
¿There is any example which uses the external CM reference?
Thank you very much,