Part Number: ADS8866
Hi Team,
Can a single buffer be used to input a +3.3V reference to multiple number of AD8866s, three, running at a 100-kSPS rate?
Thank you.
-Mark
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS8866
Hi Team,
Can a single buffer be used to input a +3.3V reference to multiple number of AD8866s, three, running at a 100-kSPS rate?
Thank you.
-Mark
Hello Mark,
This would depend on the buffer, if the Gain Bandwidth is enough to support all three ADCs at full throughput.
Will the three ADCs be sampling simultaneously? or will the conversions be staggered between the ADCs? It will be easier if the conversions are staggered.
Do you have a schematic of this?
Regards
Cynthia