< 2022.04.25 question started >
(1) For DEMOD Reg (90h - 9Fh), it seems that can't set to 3-wire mode by SPI readout. Of cource we set SENZ1=0, SENZ2=0.
We had been confirmed 3-wire readout for other registers.
Should it be possible to 3-wire mode for DEMOD Reg ?
(2) In MISC 0x2E Register VCM_FINE_PROG readout, it indicates some unclear values apart from lower 3bit.
The Reset value should be all 0.
Please tell me this behavior.
< 2022.04.28 response from Abhishek >
1. With respect to 3-wire SPI mode, are you facing difficulty in writing to demod register or reading from demod register? or both?
Generally, before reading any register, you will have to make SPI_DIG_EN pin high (since read en is not in the demod page), then set the read en. After that, if you are accessing the demod register, you make SPI_DIG_EN =0 (same as SENZ1 = 0 , SENZ2 =0)
Could you please share your sequence of operations for me to verify?
2. It is possible that register 2E [15:3] might be coming from internal fuse. So it may contain some value apart from zero. The VCM_FINE_PROG bits should be correct, thats all.
Do you read the same value in the bits [15:3] all the time or the value is different on consecutive readouts.
< 2022.04.29 answer to Abhishek >
1. Could you see an attachment ? ( DEMOD Reg. R/W test ).
I think it seems not working properly DEMOD Reg.( problem: writing and 3-wire mode reading. )
2. I can read same value from 2E so far.
Are there possibility any failure ? Or, bit[15-3] Reset Value 0h is typo in the datasheet ?