Part Number: ADS8168
Hi team,
I’ve got a question on register setting on write/read function.
On the datasheet, address is described in hex. So for example it is 1Dh (=11101 in bin) for CHANNEL_ID (Table 30), which is 5-bit.
On the other hand, on the section 7.5.2 it is mentioned the address is 11-bit.
I guess it should be right aligned, so 11101 should be 00000011101. Is my understanding correct?
Best regards,
Kurumi