Other Parts Discussed in Thread: DAC8771EVM, DAC8771
부품 번호: DAC8771EVM
I'm sorry it's a rudimentary question.
I want to check just basic DAC work through the DAC8771EVM and DAC8771EVM Software.
Using the SM-USB-DIG as the DVDD supply.
Connecting a a12V power supply to PVDD/AVDD.
And I applied all JP positions correctly.
When SM-USB-DIG is connected to PC's USB connector and DAC8771EVM software is running,
I could check SM-USB-DIG was working well.
However, there was no output from VOUT, because maybe I couldn't deal with the GUI properly.
Please help me to check just basic DAC work through the DAC8771EVM and DAC8771EVM Software.
If I didn't do anything wrong, do I need other additional hardware or software besides DAC8771 EVM?