Hello,
When we used the ADS8671 to acquire data, we were acquiring the amplifier amplified signal, the amplifier output +-12.288V signal, Vref=4.096V.
Below is the SPI waveform: adc input voltage range is +-12.288V, Vrefio=4.096V,using the default configuration. But the Vin amplitude decreased 4.5~5.5 times with the output code and LSB equation.

Best regards
Kailyn


REFIO
REFCAP
(CS)
(SCLK)
(SCLK)
(No 
SDO output with AIN_P input