Part Number: ADC128S102
Hi Team,
We received this inquiry from our customer.
We are using the ADC128S102WGRQV in a space application. During space flight a SET might occur on the OpAmp that is driving the ADC input.
During such event, the ADC input voltage might exceed the VA±0.3V so the ADC input diode might conduct for a brief period of time with a current in excess of ADC input diode 10mA rating.
Our driver could be driving up to 70mA for 2us though the ADC input diode clamp.
The 70mA diode current exceeds the 10mA ADC DC rating, but given the very short time duration (2us) we believe the heat generated in the ADC input diode will be insignificant. So exceeding the 10mA current for 2us will not damage the ADC input. Can you please confirm that?
Regards,
Danilo