Part Number: ADC32RF44
Hi Team,
This inquiry is related to the other thread. According to the datasheet of ADC32RF44IRMPT, the max height is 0.9mm as shown in the screenshot below. However, the other thread states that the height and tolerance is 0.9mm +/- 0.1mm, which would make the max on this 1.0mm. Our customer would like to confirm which one is correct. He would like to know as well what is the minimum height.
Regards,
Danilo