Part Number: AMC60804
Other Parts Discussed in Thread: AMC60304
Hi Sir,
may we know the pin define of AMC60804 and AMC60304 is the same? because seem is same package and body size.
can AMC60804 directly replace AMC60304?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Are you looking to replace AMC60304 design with AMC60804 device for only current outputs? If yes, with appropriate modifications in the schematics for GND and VCC/VSS connections, you can do that.
For more details, please connect with me over email a.k@ti.com
Regards,
AK
Hi Ak,
got it,thanks for your reply,
also,if customer do not need VDAC funciton, the AMC60304 can also directly replace AMC60804? right?
Yes, if the customer does not need the VDACs, they can directly replace with the AMC60304.