In a partial power on system. Can I power the DVDD or IOVDD without powering the AVDD? At that time I don not hope the ADC work, but I can turn on AVDD when it is needed.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
In a partial power on system. Can I power the DVDD or IOVDD without powering the AVDD? At that time I don not hope the ADC work, but I can turn on AVDD when it is needed.
Hello Xiang,
This condition will not damage the ADC, but the ADC will not work correctly after all power supply voltages return to recommended operating range. In this case, you need to assert /SYNC after all supply voltages have stabilized and /DRDY has asserted to properly reset the device.
Also note that the analog and digital input pins should not be driven before all power supplies are fully powered-up.
Regards,
Keith Nicholas
Precision ADC Applications