This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DDC264: RTD sensor array

Part Number: DDC264


Hello,

I am designing a large RTD sensor array (50+ PT1000s). I am planning on using two of these ADC daisy chained together to accomodate for my two measurement inputs and having the RTDs connected in the 4-wire configuration using a common excitation (+) and (-) for the entire array. I am looking for design/suitability advice regarding this situation. Is this ADC a good choice for this application?  Will having an external excitation source hugely affect measurement accuracy? Can I connect the excitation (-) directly to the recommended reference buffer circuit? 

  • Hi Oliver, 

    We have your ticket viewed and we'll be taking a look. Please give 24 hours for a response. 

    Kind regards,
    Nick Z. 

  • Hi Oliver,

    Not sure if you noticed that this device is a current input ADC. The inputs (single ended) are virtual grounds albeit with a sizeable input impedance (kOhms, depending on the input range).

    So, if I understand right what you are trying to do, this probably wouldn't work, isn't it? If you just wanted to measure a resistor, you could actually connect it in series between a supply/reference and the input of the DDC. The current measured would tell you the value of the resistor. There are probably other variations of that approach but not sure you would get all what you usually get with the 4-wire configuration (differential measurement, cable resistance not affecting the measurement, etc). I haven't seen it done with a DDC. Would have to think about it but probably a no-go?

    Regards,
    Eduardo