Part Number: TSW14J56EVM
Other Parts Discussed in Thread: TSW54J60EVM, ADS54J60
Hello,
I'm currently using the TSW14J56 eval board (labeled "PCB REV E") with the TSW54J60EVM (Rev B) ADC board. Using the HSDC Pro (v5.20) software (both directly and via the Matlab automation interface), I'm able to capture data from the ADC without issue, including with a single external trigger. However, when I select the option to auto re-arm the trigger and choose some number of triggers, the device no longer seems to see the triggers and won't capture data. If I click the "Show Trigger Status" button, the status box that shows up likewise indicates that no triggers have been seen ("Number of Triggers Occurred" stays at zero), regardless of how many external trigger signals I send.
Are multiple, auto re-armed trigger captures supported for these boards?
I'm ultimately interested in capturing short, triggered bursts of data, say around 100 microseconds, for triggers that are separated by many milliseconds.
Thanks,
Brian