This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TSC2013-Q1: REGISTERS FOR SINGLE TOUCH AND CALCULATION OF COORDINATE

Part Number: TSC2013-Q1


Hello team,

1. Which registers should we consider o understand the position of the touch in single touch configuration using the TSC2013-Q1 device? Is it (X1,Y1) or(X2, Y2)

2. Which mode is used in the eVM? Is it TSMODE1, TSMODE 2 OR TSMODE 3?

3. How can we get exact coordinate on the touch screen as an output of TSC2013-Q1?

Request your inputs! 

This is very urgent and is running at customer end for three weeks now. Request priority response!