This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS7952: SDO output pin characteristics of the SPI bus

Part Number: ADS7952


Hi,

We are setting up a schematic diagram with an ADS7952 (38 pins tssop package) based on SPI communication.

The SPI bus in this design is shared with other slave devices where each slave device can talk back to the

microcontroller as well. This means that in our design all SPI slave devices should be connected with their

SDI signals together, as is the case for all SCLK signals.

However the SSEL output (chip select output) of the microcontroller is connected to a 3-to-8 demultiplexer.

Basically the questions are about the SDO  pin :

1) Has the SDO pin of the ADS795x a default (fixed) defined logic level (either "0" or "1") when the chip select

pin = "1" (SPI bus of the chip is deactivated) ?

  In a shared  SPI bus this means that each SDO pin of an SPI slave device should be connected to some form of

 input (or protection) for instance an input multiplexer or  tristate buffer.

2) Perhaps in general : should each SDO pin of (all) SPI slave devices of TI be connected with some form of input

(or protection) this way ?

Thx in advance,

Armand

  • Hi Armand,

    After the 16th SCLK in the frame, SDO goes into a high impedance state (tristate). Because of this, you should be able to connect other SDO's to the ADS795x and any other protection shouldn't be needed. You can observe the time it takes for SDO to go into a high impedance state by looking at td3 in the timing diagram below taken from the data sheet.

      

    Regards,

    Aaron Estrada