This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1261: ADS1261BIRHBR vs ADS1261BQWRHMRQ1

Part Number: ADS1261


Hi,

I've looked and cannot find anything to decode the TI part number and would like to know the difference between:
ADS1261BQWRHMRQ1

and 

ADS1261BIRHBR

It is clear the device package is different but otherwise I'm not clear on what the other differences are. 

Thanks,

Tyler

  • Hi Tyler,

    welcome to our e2e forum and thanks a lot for your interest in our ADS1261.

    I can help you decode the letters after the "ADS1261B".

    • First letter is the temperature range indication.
      "Q" stands for the automotive temperature range from -40°C to 125°C
      "I" stands for the industrial temperature range but can be -40°C to 85°C, 105°C or 125°C
    • The next few letters are the TI package designators.
      "RHB" for the 32-pin QFN package
      "WRHM" for the wettable flank 32-pin QFN package
    • Thereafter follows the carrier type.
      "R" in this case indicates a large tape&reel.
    • "Q1" indicates that this device is AEC-Q100 qualified for automotive applications

    The main difference between the two devices is that one device is the version qualified according to AEC-Q100 for automotive.
    Both devices have the same features and functionality. There might be slight differences in the MIN and MAX parameter specifications.

    Regards,
    Joachim Würker

  • Thanks Joachim this is exactly what I needed to know