Part Number: ADS54J69
Hi,
I'm trying to run the ADS54J69 in 2242 mode. But when I checked the jesd interface before programming the IC, I saw that the sync pin was constantly dropping. I connected gt_rx output ports of jesd204_phy ip and rx_sync output port of jesd204c ip to ILA to control the interface. You can see the ILA signals in the link below.
https://drive.google.com/file/d/1w1p4Aho0rXOFXa1VBDct8O40oVJKuxI4/view?usp=sharing
After programming the IC (after setting its registers), the adc data is not valid at all. The rx_tvalid (adc1_data_v) signal is always 0. I can not get data from ADS54J69. You can see the ILA signals after programming the IC from the link below.
https://drive.google.com/file/d/1ksrOjkzABmbQdEHM21rfCxLO4knk-68H/view?usp=sharing
Line Rate = 5Gbps
Reference Clock = 125 MHz
I configured the registers of ADS54J69 as follows:
600001
600000
000081
000080
005920
400100
400200
400468
400300
60F701
600001
600000
400469
400300
600080
60060F
600580
600102
60310A
60320A
40046A
400300
601602
601B08
601A02
400468
400300
604112
604D08
605280
607208
600001
600000
Why is the sync signal constantly dropping? Why is the data valid signal not high after programming the IC? Can you help me?