Part Number: DAC3482
Hello,
We use two DAC3482 our system. We control these DACs with Xilinx's Zynq series. The LVDS line of the first DAC is connected at bank 1.8V and the second dac is connected to the LVDS 2.5V bank. The first DAC works fine. It passes the IO Test pattern without any problems. But the second DAC is not works. Hardware, digital design and SPI configurations are exactly the same. Do we need to apply LVDS strength to fix this situation? Will LVDS_25 damage DAC's LVDS inputs?
Thanks you TI Team.