I have a question in the user manual provided to interface the MCU of another board using the AFE of the EVM.
In the case of the CLK pin, the manual says "Pad of R11 that is not connected to GND".
When internal oscillator mode is applied in AFE,
In the EVM kit, it seems that the CLK resistor is removed, so it does not give a CLK signal.
I want to know if it is necessary to use CLK on other boards.