This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC7573: The difference between TR and DR

Part Number: DAC7573
Other Parts Discussed in Thread: DAC63204

Hi Team,
I have several questions about the DAC7573.
There is a temporary storage register (TR) and a DAC register (DR) for setting the output voltage. Are they volatile and non-volatile, respectively, or are they both volatile?
In the explanation of power-on reset, the DAC register is filled with zero and the output voltageis 0V on power up.
I want to power up with the output voltage set in the register, but if this is not possible, what is the difference between TR and DR?
If I don't use an external timing signal for updating, is the LDAC pin connected to either VDD or GND? Or does it keep open?
Best regards,
Nakayama