This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE4300EVM-PDK: Electrode probes that are used with this PDK

Part Number: AFE4300EVM-PDK
Other Parts Discussed in Thread: AFE4300

Hello,

I am designing a Weight scale and body composition device using AFE4300, for which i have bought the AFE4300EVM-PDK to understand the functionality.

So, I need to know what kind of electrodes are used with it.  Can you refer any electrode.

Also i have 10 lead ECG electrode, will that work if i used LL, RL, RA, and LA from it.

Also i need to know how to connect LL, RL, RA and LA with the AFE.

Is Wet of Dry electrodes used with this ?