Part Number: ADS8866
Other Parts Discussed in Thread: ADS8699,
Howdy!
I need to use industrial sensor for position sensing. It has 0 - 2.5V analog output. I was looking for some simple ADC capable of following parameters to digitalize the signal:
Vin = 0-2.5 V
>16 bit resolution
>10kSPS
SPI interface
I found following ADCs:
https://www.ti.com/product/ADS8866
https://www.ti.com/product/ADS8699
I would like to ask which is more suitable for the operation. Either to use higher resolution ADC (18bits ADS8699) with only using half of the input voltage (±2.5V using +2.5V only) OR to use single ended capable ADC with (16 bits ADS8866) with Vref 2.5V. What would you recommend?
Thank you,
Best Regards,
Michael