Part Number: ADS1261
Other Parts Discussed in Thread: ADS124S08
I hope you can support us on following issue:
the ADC is to sample synchronized to an analog signal from the microcontroller. The synchronization is solved by a shared clock between ADC and microcontroller. For this purpose it is important to know the timing of the ADC exactly in order to synchronize the signals. During this task several problems or questions came up, which we would like to clarify.
Questions about the behavior of the ADC:
- Is it basically allowed to use other frequencies - Basically the datasheet gives a range in which the ADC can be operated. However, other data sheet passages explicitly refer to 10.24 MHz or 7.3728 MHz (chapter 9.4.4).
-Is the calibration capability given for frequencies not equal to 10.24 MHz or 7.3728 MHz (see data sheet chapter 7.3)? How long does the calibration take for deviating frequencies?
- The application note linked to the ADS1261 gives many hints about the conversion latency, but not much is said about the calibration time. Currently, our measurements of the calibration time do not provide reproducible results. This results in inconsistent results when recording the calibration time.
- How does the conversion latency depend on the input frequency? Is there an exact breakdown?
- The application note states that the sampling time basically consists of a programmable delay, the actual sampling time and an overhead. On the one hand, the question is whether a delay of 50 uS also scales with the clock frequency, and on the other hand, how the overhead is composed (for example, there is information for the ADS124s08 in the application note as a table, something like that would be very helpful)
- The datasheet talks about a 4th order Delta Sigma modulator, one question is what exactly the 2+2 pipelining means for the application (or the question: Is this relevant for our application?).
- What is the exact calculation basis of the sampling rate depending on the clock? Does the calculation basis work for the whole range, i.e. also for very low frequencies? For example, if a clock of 1 MHz is set at 40 kSPS I had to split the answer, because of the limitation in text field.
If you have any technical questions, please contact Mr. Will-Groo directly (paul.will-groo@ifm.com).
Best regards Dominik Schlachter