Part Number: ADC121S021
Other Parts Discussed in Thread: ADS7042
HI staff
In the current app, the NJL7502R phototransistor is directly connected to the analog input terminal of the LTC2361.
ADC121S021 is selected instead of ADI's AD converter.
The ADC121S021 does not have a buffer on the analog input. Is it okay to connect the tactile sensor?
Also, I would be grateful if you could introduce a device that is suitable as an alternative.
(It is especially important to have a small pkg)
NOTE:
At first, I chose ADS7042 as a candidate, but I excluded it from the candidates because a buffer amplifier is required before AD.
best regards
cafain